Steel Mills
The Best Gearbox, The Fastest Response
Bill Sutton, SMA SalesWith unclear delivery commitments from its former gearbox supplier and after successful trial runs with Sumitomo gearboxes, Nucor contacted Sumitomo to supply the remaining phase of their project with an additional 35 gearboxes. Within two weeks of facing a standstill in their operations, Sumitomo reassured Nucor that they would receive their order in time. Not only did Nucor receive their extra order of gearboxes, they were delivered in an amazing 5 days! Representative of Nucor, Chris Kovalsky said, “With respect to our issue, I could not be more pleased with the responsiveness Sumitomo displayed. Their gearboxes will be getting installed on the next four phases of this project.”
For over two months Nucor has been using 40 Sumitomo gearboxes in reversing applications under heavy loads, without incident. Now, with the assistance of the Sumitomo Cyclo® 6000, Nucor Steel can continue producing steel sheets without the stress of possible gearbox failure. Once Nucor completes its tunnel furnace upgrades, they will have more than 200 Cyclo units installed in their Arkansas factory. Sumitomo Cyclo 6000 provides both a cost effective and highly efficient gearmotor for Nucor Steel.
The Sumitomo Cyclo 6000 series gearmotors are available from 1/10 to 235 HP and ratios from 3:1 to 658,503:1. The gearmotors are maintenance free, lightweight, compact and very rugged with a two-year warranty guaranteeing exceptional performance. For more information, please contact 1-800-SM-CYCLO or email us.

EN ▼