Packaging

Packaging Machinery

Automation of Lowerator: HYPONIC® Gearmotor

Josh Carney, Olivia Martin


Challenge
The automation plant redesigned its application. From a single gearbox running two shafts using a series of chain, sprockets, and idlers, the new configuration called for a direct drive system with one gearmotor for each shaft, vertical shaft down. There are a total of five of these systems in the plant.
First, it was redesigned utilizing a competitor's worm drive reducer, which lasted one week before leakage and failure. In an attempt to resolve the situation, our competitor recommended an increase in the size of the reducer. This improved the situation; however, reducers were still failing within 4 to 5 weeks. The customer noted that the reducers were running extremely hot and constantly leaking. The customer had to issue 25 work orders over the course of the year, which led to durations of 1.5 to 3 hours of downtime per repair.

Solution
The solution was the grease-lubricated, HYPONIC® Gearmotor Model RNYM 1-1520YC-F1-60. Due to the smooth, almost frictionless operation of the HYPONIC®, torque is transmitted more efficiently, producing less heat than a conventional worm gear. Also, the grease lubrication feature allows the reducer to be mounted universally and is virtually maintenance-free.

Results
Sumitomo negotiated a 60-day trial of the proposed gearmotor. Once it was installed, the customer monitored daily amperage draw and temperature of the HYPONIC®. Within the first 30 days, the customer was so impressed with the unit's performance that the plant invited Sumitomo Machinery Corporation of America for a meeting to discuss replacing all 10 drives. Sumitomo met with the customer nearly once a month to quote replacements on existing drives in other applications, as well.

"At first, some were asking why we were spending more than we usually do on gearboxes. Now that they have seen the benefits of using Sumitomo, I am getting requests for your product in other locations. Upgrading to the HYPONIC® has virtually eliminated all preventative maintenance and downtime. No work orders have been issued since the switch." -HYPONIC® Customer, Champaign, IL.

hyponic cs1.jpg

hyponic cs2.jpg


Case Studies



Locate Your Nearest Representative

Our comprehensive sales and service network extends throughout North and South America. Enter your zip code to find the Sumitomo facility, sales representative, and distributor in your region.

Configurator

Sumitomo's product Configurator is live! Select the ideal Sumitomo product for your application, download 2-D and 3-D CAD drawings and models, and print out a technical spec sheet of your configuration!
Click here to get started! Sumitomo's Product Configurator

Website Feedback

Do you have questions or comments regarding our website? Click below to submit feedback!

Submit your comments here>

;