Chemical

Chemical

In our environment, it's about reliability. The Cyclo is the most reliable reducer in the market. With the Cyclo, there is no catastrophic failure. They just begin to get noisy, allowing us to stand by the reducer and replace it when it's convenient to us. It's been a good partnership with Sumitomo all around: from the local salesperson, to the technical support, to the customer service in Glendale Heights.

Parcel Handling

Cleveland, OH


Our customers originally introduced us to Sumitomo via their specifications. Upon using Sumitomo for many successful projects, we adapted Sumitomo Cyclo and BBB as our standard. We have utilized Sumitomo reducers for many demanding applications and to date have not had a single failure or warranty-call related to the reducers.

Automotive
Automotive Mechanical Lifter Manufacturer
El Segundo, CA


Paramax drives match our own demands for durability and reliability in a product...Sales engineers work closely with our designers to come up with precisely the drive we need for a given application. When you take on the responsibility of lifting and moving heavy loads--up to 250 tons--you want every component in the system to do the job it was intended to do; smoothly and reliably and, above all, safely. Sumitomo Paramax drives have proven extremely reliable in every one of the cranes for which it was specified.

Crane & Hoist

Ashland, VA


Paramax reducers were initially specified for this application for off-the-shelf availability of internal parts. Little did we know that spare parts would not be needed. The Paramax units run cooler, quieter and more reliable than any we've had in the past.

Waste Water Treatment

Clearwater, FL


Cyclo drives have given us the best performance of any of the gear drives we've ever had in this plant. Not only have we noticed a 40% reduction in amp draw over previous units, we find that our mixers are distributing wastewater to all corners of the tank. This tells us that the Cyclo Drives are using less energy while supplying more torque than we used previously.

Waste Water Treatment

Hillsborough County, FL


Our first experience with Sumitomo was very convincing. A gearmotor was failing periodically on a horizontal rotary furnace at one of our installations. The application was particularly demanding. Production schedules at the installation would not always allow maintenance when needed and the gearmotor was subjected to high heat, abrasive dust, and an uneven (at times pounding) load. At the time, we were using a very large and robust drive from a well-known US manufacturer. Sumitomo suggested a Cyclo drive that was very compact. In fact, it was so compact that my first impression was to reject it without even a trial. In the end, we did install it and it has served since, without any fail, for decades. I was surprised that such a small compact drive could so complely outperform its much larger predecessor.

Mineral Mining

Chadds Ford, PA


Our applications are so demanding that we've broken shafts, we've broken pillow blocks, but we've never broken a Cyclo reducer. In one case, the gears of one of the previous drives flew right out of the casing when shock pounded the worm right through it. Now, anytime a drive in the plant failed, whenever possible, we replace it with a Cyclo. Cyclo tolerates harsh operating conditions like rapid reversal, shock loads, water, dirt and heat better than any other gearbox.

Steel Mill

Whitby, Ontario


When you need these high-reductions in a compact, durable, low-maintenance package, Cyclos are really the only choice. We specify Sumitomo for every critical appliation requiring drives and controllers.

Elevator
Elevators, Escalators, Moving Walkways
Newport News, VA


We've switched over to gears based on cycloidal discs for all our indexing equipment. With conventional gears, the constant starting and stopping would break down the motor windings.

Packaging
Beverage Case Packer
Hightstown, NJ


We have over 20 miles of belt conveyors, some up to five feet wide, move the packages through a complex network at speeds to 400fpm. When you move those volumes at those speeds, you need to avoid a drive breakdown. We choose Sumitomo Cyclo speed reducers because problems often associated with toothed gears are precluded.

Parcel Handling

Memphis, TN


Locate Your Nearest Representative

Our comprehensive sales and service network extends throughout North and South America. Enter your zip code to find the Sumitomo facility, sales representative, and distributor in your region.

Configurator

Sumitomo's product Configurator is live! Select the ideal Sumitomo product for your application, download 2-D and 3-D CAD drawings and models, and print out a technical spec sheet of your configuration!
Click here to get started! Sumitomo's Product Configurator

Feedback

Do you have questions or comments regarding our website, products or services? Click below to submit feedback!

Submit your comments here>